Use of Ringo software in tea2017?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use of Ringo software in tea2017?

2,097件の閲覧回数
Jayler
Contributor I

1. Can the new TEA2017 chip be used directly without software configuration?

2. There are two groups of signals from I2C, which are connected to the device and the development board. What is the difference between the two in software configuration?

3. Is there any other way to buy rdk01db1563 in China? The official website has been sold out.

0 件の賞賛
返信
3 返答(返信)

2,094件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

1: Yes,you can!
2:which point do you mean? 

3:contact with your local NXP distributors:Distributor Network | NXP Semiconductors

0 件の賞賛
返信

2,090件の閲覧回数
Jayler
Contributor I

about 2:I can configure tea2017 with tea2017dk1002 or directly on the  power board. What is the difference between the two methods?

thank you!

0 件の賞賛
返信

2,075件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Depend on your side,you also can directly program it in your power board.

0 件の賞賛
返信