Ucode8 EPC Session Timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ucode8 EPC Session Timing

1,459件の閲覧回数
justin_andrews2
Contributor I

I'm trying to determine what the session times are for the Ucode8.

Per the EPC standard, the Session flag S1 should be between 500ms and 5000ms, and the Session flag S2/S3 and SL should be greater than 2s.

Is there a  spec or characterization of these EPC session timings for the Ucode8?

0 件の賞賛
返信
1 返信

1,439件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @justin_andrews2 ,

 

UCODE 8 comply with the following spec:

Kan_Li_0-1640149782241.png

Please kindly refer to https://www.gs1.org/sites/default/files/docs/epc/Gen2_Protocol_Standard.pdf for more details.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信