Hi NXP Team, We have two batches of boards that use the same UJA1169AXF and identical firmware, but they show different CW-flag timing after CAN wake-up: Event
Board-A sequence Board-B sequence Board A When the second wake-up frame is sent, V1 rises to 5 V, yet the CW flag in register 0x63 remains 0. Only after the third wake-up frame does CW become 1.
Board B With the second wake-up frame, V1 rises to 5 V and CW is already set to 1; no third frame is needed.
Could you explain what on-board parameter makes the CW bit wait for an extra frame on some boards? Is it related to V1 rise time, PNP load current, or another analog threshold that gates the internal “wake-up confirmed” signal?
Thanks for any hints!
Best regards, Zhaoguanyu