Hi,
I have recently taken ownership of a legacy project, one of the components is a M68HC16Z1EVB board and some custom software. It did not come with any software or manuals. I was able to find a second such board on ebay which came in the original packaging. I bought it and the manuals have been very helpful. The software came on a 5.25" disk which I sent to a data recovery company but sadly some of it was too corrupt to be retrieved.
I would like to find a working copy of the software - most importantly the debugger (which seems to connect via an old-style parallel port) and the assembler (although I see there are some open source alternatives around).
Can anyone help me find a copy?
Thanks in advance.