The debugger to work with NXP Processors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The debugger to work with NXP Processors

3,417 Views
kumar_086
Contributor IV

Dear NXP Team,

We are having the custom boards housing multiple variants of NXP Processors namely, MPC864x, QorIQ T/P series, Layerscape series. Can you recommend a common debugger which can work with all the processor architectures?

Checked the CW-TAP - https://www.nxp.com/design/design-center/development-boards-and-designs/CW_TAP - but its not having the MPC864x and QorIQ P-series as per the supported devices list shown.

Regards

Tags (1)
0 Kudos
Reply
7 Replies

3,387 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello, 

the CW TAP (CWH-CTP-BASE-HE) supports all the mentioned processors. 

Oswalag_0-1726687536566.png

 

BR,

 

0 Kudos
Reply

3,376 Views
kumar_086
Contributor IV

Hi,

Thanks for your reply.

Based on the link - https://www.nxp.com/design/design-center/development-boards-and-designs/CW_TAP : the PPC - MPC864x series like MPC8640/MPC8641 is not shown on the page. Can you clarify on this processor set?

Regards

Tags (1)
0 Kudos
Reply

3,359 Views
Oswalag
NXP TechSupport
NXP TechSupport

It isn't mentioned but the USB TAP CWH-CTP-BASE-HE with CWH-CTP-COP-YE Probe Tip could be used with MPC864x processors.

0 Kudos
Reply

3,349 Views
kumar_086
Contributor IV

Hi,

When the Code warrior tool is installed, the MPC8640 is not found in CW versions v10.4.0, v10.5.1. Please let us know if we need to enable any additional patches/updates. Shared the snapshots of processors of both versions.

 

kumar_086_0-1726829275668.png

 

kumar_086_1-1726829401889.png

Regards

0 Kudos
Reply

3,309 Views
Oswalag
NXP TechSupport
NXP TechSupport

It is because MPC864X is not supported by Code Warrior for Power Architecture IDE, it is supported in CodeWarrior 8.8 (IDE 5.9). 

0 Kudos
Reply

3,269 Views
kumar_086
Contributor IV

How do we download this version? Can you help us with the link details?

0 Kudos
Reply

3,186 Views
Oswalag
NXP TechSupport
NXP TechSupport
0 Kudos
Reply