Tensorflow lite buil problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tensorflow lite buil problem

937件の閲覧回数
EPellegrino
Contributor I

Dear all,

I am working on https://www.variscite.com/product/evaluation-kits/dart-mx8m-plus-evaluation-kits/ which mount a iMX8M Plus with custom debian distribution based on Bullseye (kernel 5.10.52_2.1.0)

I am trying to build from source Tensorflow lite (https://github.com/nxp-imx/tensorflow-imx) but I am having problem in bazel phase. My current setup is:

  • branch: lf-6.1.55_2.2.0
  • bazel version 5.3.0
  • clang-llvm16.0.0-aarch64-linux

After configuring build and running bazel as per documentation (https://www.tensorflow.org/install/source) I get:

ERROR: /run/media/system/mmcblk1p1/tensorflow-imx/tensorflow/cc/saved_model/BUILD:91:11: Illegal ambiguous match on configurable attribute "deps" in //tensorflow/cc/saved_model:loader:
//tensorflow:framework_shared_object
//tensorflow:elinux
Multiple matches are not allowed unless one is unambiguously more specialized.

What could be the problem?

0 件の賞賛
返信
1 返信

925件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @EPellegrino!
Thank you for contacting NXP Support!

Try to compile the branch "lf-5.10.52_2.1.0" for your board.

If that doesn´t work contact to variscite to get support in that

Best Regards!
Chavira

0 件の賞賛
返信