TJA1153

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TJA1153

2,563 次查看
raztiko
Contributor I

The TJA1153 supports 500Kb according to the datasheet

 

Is there a secure CAN Transceiver that supports 1Mb? If not, Is there a roadmap for pin compatible device that is a secure CAN transceiver up to 1Mb?

 

 

0 项奖励
回复
4 回复数

2,531 次查看
YoavBY
Contributor I

Hi, thanks for the reply.

We are looking into the secured transceivers. However, per 1153 datasheet seems that can support arbitration rate of up to 500 Kbps and not 1 Mbps

• Operates in Classical CAN and CAN FD systems with arbitration phase bit rate set at
125 kbit/s, 250 kbit/s or 500 kbit/s

(also per CAN_CANFD_BR settings)

In NXP roadmap - is there intension to support 1 Mbps of arbitration rate?

 


• For arbitration bit rates of 250 kbit/s and 500 kbit/s, the fast phase bit rate can be set to
two or four times the arbitration bit rate

0 项奖励
回复

2,553 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Raz,

for our CAN transceivers portfolio please refer to this link. The TJA1153A supports data rate up to 5Mbit/s. 

JozefKozon_0-1691052163342.png

With Best Regards,

Jozef

 

0 项奖励
回复

2,454 次查看
YoavBarY
Contributor I

Hi, thanks for the reply.

We are looking into the secured transceivers. However, per 1153 datasheet seems that can support arbitration rate of up to 500 Kbps and not 1 Mbps

• Operates in Classical CAN and CAN FD systems with arbitration phase bit rate set at
125 kbit/s, 250 kbit/s or 500 kbit/s

(also per CAN_CANFD_BR settings)

In NXP roadmap - is there intension to support 1 Mbps of arbitration rate?

 


• For arbitration bit rates of 250 kbit/s and 500 kbit/s, the fast phase bit rate can be set to
two or four times the arbitration bit rate

0 项奖励
回复

2,447 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Raz,

I apologize, I misunderstood you. Unfortunately no. We do not have a CAN transceiver with Arbitration rate of 1Mbit/s and there is not any planned. I apologize for inconvenience. 

With Best Regards,

Jozef

0 项奖励
回复