TJA1102- Power mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1102- Power mode

1,136 Views
Lukas4
Contributor I

Hey,

i try to change the power mode of the TJA1102 from normal op to standby mode. Therefore I activated the "CONFIG_EN" Bit (Register 17, bit 2). However I can't change the power mode.

Do i have to change other registers before I can change the power mode?

Thank you for your help.

 

Your's

Lukas

0 Kudos
Reply
1 Reply

879 Views
Markovic
Contributor I

To achieve this, I was updating Extended control register (register 17), POWER_MODE [14:11] field.
Writing Sleep Request command to the field (= 1011 ) the PHY would go to sleep mode (reading the register 1010 could be seen on the filed).
Also, basic conditions for sleep mode should be achieved - no WKU requests detected, no traffic (or the PHY is configured not to be influenced by those)

0 Kudos
Reply