TJA1043 Communication Abnormal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1043 Communication Abnormal

934 Views
caesar_song
Contributor III

Hi Guys

   Regarding the transceiver of TJA1043, will it enter an abnormal state if there is an exception on the CAN bus? How does it behave once it's in an abnormal state? For example, can packets be sent but cannot be received,thanks

Tags (1)
0 Kudos
Reply
1 Reply

925 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Caesar,

could you please elaborate what you mean by the abnormal state? There is five modes/states in the TJA1043, which are controlled by STB_N, EN pins and be the wake-up event. 

JozefKozon_0-1739947446824.pngJozefKozon_1-1739947464044.png

Please elaborate on what you mean an exception on the CAN bus. Do you mean the CANH or CANL, or both are short circuited to VBAT, VCC or GND? If yes, there is a description of this fail in the section 7.3.3 in the TJA1043 datasheet. 

JozefKozon_2-1739947597230.png

 

With Best Regards,

Jozef

0 Kudos
Reply