TJA1028TK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1028TK

1,496件の閲覧回数
Nihplodic
Contributor I

What is the difference between these two suffixes?

TJA1028TK/5V0/20/1    and 

TJA1028TK/5V0/20/2

Anyone?

0 件の賞賛
返信
2 返答(返信)

1,492件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jacky,

TJA1028TK/5V0/20/2 is not an orderable part number, it seems to be a typo.

If you meant TJA1028TK/5V0/20/J, then the packing type (tape & reel 13 inch) is identical with the TJA1028TK/5V0/20,1.

The only non-technical difference is that /J indicates our dual sourced device. This is to help protect from supply chain interruptions that could occur due to natural disasters. 

Best regards,

Tomas

0 件の賞賛
返信

1,484件の閲覧回数
Nihplodic
Contributor I

Thanks Toby,

Requesting a picture of the label from vendor...

0 件の賞賛
返信