TJA1028

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1028

2,551件の閲覧回数
girishmallappa
Contributor I

Application circuit diagram for TJA1028 LIN & TJA1042T CAN Transceiver part

0 件の賞賛
返信
2 返答(返信)

1,935件の閲覧回数
stephen01
Contributor I

Hi I have some questions about the TJA1028

1> What is the direction of the RSTN pin from TJA1028. It is input or output?  My circuit let this pin float. Is it ok? 

2> VCC PIN is output or input of the TJA1028

3> If my system does not need this power, the VCC pin is in float status, R226 resiter is no on board, V3.3 is not connect with VCC .  it is OK? 

4>   If TJA1028 work as Master, the LIN bus connect CAP is 220pF.   Is it OK?  If the TJA1028 work as Slave, the CAP value is? 

 

thanks for you help solving these questions.

       LIN_MASTER.JPG

タグ(1)
0 件の賞賛
返信

2,422件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Girish,

Below you can find a typical LIN slave application with the TJA1028.

pastedImage_1.png

Hope it helps.

Best regards,

Tomas

0 件の賞賛
返信