TJA1021 bug...?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1021 bug...?

8,781件の閲覧回数
gicking
Contributor I

hello all,

in a project I use a TJA1021 LIN transceiver. Today I found something weird, which seems to deviate from the state diagram on page 6 in the TJA1021 datasheet. Maybe you can explain that to me...

In my circuit the pins are connected as follows:

  • RXD <-> µController Rx with 10k pull-up to 5V
  • TXD <-> µController Tx
  • SLP_N <-> 5Vreg --> no sleep used
  • WAKE_N <-> open
  • INH <-> open
  • Vbat <-> supply voltage (normally 12V)
  • LIN <-> LIN bus with 1R pull-up to Vbat

If I switch on Vbat=12V, everything works as expected. However, if I first plug in board USB (Vbat~4.4V) and afterwards Vbat=12V supply, there is no traffic on LIN or RxD. The µContoller is sending via TxD, but neither LIN nor RxD show any activity. I checked with an oscilloscope, and see TxD is active, LIN static at ~12V, and Rx~5V. Also, manually connecting LIN to GND (-> bus wake) has no effect.

The state diagram on page 6 in the TJA1021 datasheet shows that the chip switches to normal mode if SLP_N=HIGH, independent of the initial condition. But apparently that is not the case. What am I missing...? 

I searched the internet but found no errata or other report of this strange behavior. Any help is highly appreciated! Thanks a lot in advance!

Regards, Georg

タグ(3)
0 件の賞賛
返信
2 返答(返信)

8,377件の閲覧回数
Tarloth
Contributor I

Please @dietmarschmid , can you answer here to this post, I like to see the answer to this problem. Thanks

0 件の賞賛
返信

8,756件の閲覧回数
dietmarschmid
NXP Employee
NXP Employee

Hello Mr Icking,  think this was answered already by me via tec support

0 件の賞賛
返信