Hello, I am trying to implement remote wake up with the TJA1055T/3z integrated circuit. After putting the integrated circuit into sleep(0-1) mode, I transition it to sleep(0-0) mode. When I attempt to send a CAN message, I cannot detect any change on the ERR pin, and my VECTOR device that I'm using encounters an error. What could be the reason for this? (I am supplying 5 volts to the VCC pin, and I have pull-up resistors on the ERR-RX-TX pins with power supplied to them as well). What steps should I follow to achieve remote wake-up
Hello Yiğit,
please share your schematic with voltage levels and part values. How have you connected the INH pin?
With Best Regards,
Jozef
Hello Yiğit,
thank you for the additional information. Please share the schematic with voltage levels and part values. Also please share the scope from the CANH and CANL bus. If the remote wake-up pattern is correct.
With Best Regards,
Jozef