TJA 1043 CAN link down error/ Chip state error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA 1043 CAN link down error/ Chip state error

1,619 Views
Thiru09
Contributor I

Hello Team,

 

We are using TJA 1043 CAN transceiver in our design , during the BCI tests between 1- 40 MHz we get the Link down and chip state error. To fix this i would like to understand the below factors

1. In which condition the link goes down --> interrupting CAN H/L bus or INH or any other pins could cause the link down issue?

2. Are there any lessons learnt from BCI issues with TJA 1043 already available?

 

Thanks

Tags (3)
0 Kudos
Reply
3 Replies

1,590 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

What do you mean about link down? do you mean the CAN communication failed?

We didn't see such failure before.

 

0 Kudos
Reply

1,584 Views
Thiru09
Contributor I
Hi, Yes the Communication is down and also chip state errors received,
- If not seen before is it possible to explain--> "if which pins gets disturbed to get this scenario happen?"
0 Kudos
Reply

1,580 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

You need to catch some waveforms during failure happened including CANH/L/STB_N/EN.

0 Kudos
Reply