TFF1003HN을 사용하려구 합니다

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TFF1003HN을 사용하려구 합니다

853 次查看
윤선우
Contributor I

TFF1003HN에서

REF 50MHz를 줘서 출력주파수 (LO) 13.05GHz를 만들수가 있나요?

0 项奖励
回复
1 回复

792 次查看
alexander_yakov
NXP Employee
NXP Employee

TFF1003HN is Voltage-Controlled Oscillator (VCO), which generates output frequency in range from 12.8 to 13.05.

This output frequency is internally divided by divider and output of this divider is compared with reference input frequency.

Possible divider values are: 256, 128, 64, 32, 16

If your reference input frequency is approx. 50Mhz than you should use divider value - 256.

Please look TFF1003HN device datasheet, Table 8:

http://www.nxp.com/documents/data_sheet/TFF1003HN.pdf 

In this table you can see that for divider ratio 256 you can have input frequency in range from 50.000 to 50.997

So, for fixed divider rate "256" there will be:

for input frequency 50.000 Mhz: 

50.000 * 256 = 12800 Mhz

for input frequency 50.997 Mhz:

50.997 * 256 = 13055,232 Mhz

In other words, for output frequency 13,05 Ghz yu have to use input reference frequency ~50.997 Mhz.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复