TEA1916 LLC transformer getting hot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA1916 LLC transformer getting hot

939 Views
juliocruz
Contributor III

Hello,

I builded a SMPS based on the TEA1916 combo and following the example TEA1916DB1262UL. 

The current output limit is set accordingly (based on TEA1916 power limit) to 140W and is working as expected.

The output voltage is set to 16V. 

The LLC transformer is getting hot (80 degree celsius) when the load is 50W.  Everything else (mosfets and bridged diodes) seems ok. 

Please, may I know which parameters may I change in order to reduce the transformer temperature?

Additionally, It's this temperature expected without force ventilation?

Thanks 

0 Kudos
Reply
2 Replies

849 Views
juliocruz
Contributor III

Hi Sun,

The transformer temperature rise in full load is ~95C after 20 minutes.

I just modified the transformer and get better results.

Thanks

0 Kudos
Reply

849 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Could you please let us your product safety standard level?

What's your transformer temperature rise in full load?