TDA8954TH BTL Mode Module Board AU BTL Output interference

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TDA8954TH BTL Mode Module Board AU BTL Output interference

2,790件の閲覧回数
gbowman
Contributor I

I am using a TDA8954TH BTL Mode Module Board AU for some prototyping work and have a condition which I am struggling to resolve. 

The TDA is connected in BTL mode. As I increase drive to the board there is a point where I get severe "break up" as per the attached pic.

The two traces are showing the + and - outputs of the BTL. The signal appears on both traces at the same time.

It does not appear at all until about half max output. Interestingly it is not there when I do not have a load connected.

As best as I can measure this the break up signal is around 40KHz... not the (~300KHz) of the PWM.

It also seems that it occurs earlier with low frequency signals... i.e. more prevalent at 100Hz than 1KHz upwards.

Any suggestions much appreciated. 

TDA8954TH BTL Output.jpg

3 返答(返信)

2,697件の閲覧回数
gbowman
Contributor I

Sorry… I am struggling to find out how to move or delete it... suggestions please?

0 件の賞賛
返信

2,697件の閲覧回数
Ragan_Dunham
NXP Employee
NXP Employee

Graham, we will move the post for you. Thanks!

2,697件の閲覧回数
manish_bajaj
NXP Employee
NXP Employee

[email protected]‌,

You have posted ticket in wrong community.  This community is dedicated for eIQ support.

0 件の賞賛
返信