Spice model for BFU910F Transistor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Spice model for BFU910F Transistor

跳至解决方案
2,665 次查看
huiyanhuan
Contributor I

Hi, 

I would like to request for the Spice model file for BFU910F, could you please send it to my email address? 
Thank you.

0 项奖励
回复
1 解答
2,434 次查看
LPP
NXP Employee
NXP Employee

Sorry, we have no spice model for the BFU910F, only ADS model for nonlinear simulations, for linear S-parameters are available.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,435 次查看
LPP
NXP Employee
NXP Employee

Sorry, we have no spice model for the BFU910F, only ADS model for nonlinear simulations, for linear S-parameters are available.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,434 次查看
mhu
Contributor I

Hi,

I also would have required a non linear model for spice or qucs for BFU910F.

In the TDS it is stated that a spice model based on Gummel-Poon model is avalaible from Q1 2015.

Does it mean the TDS is in inaccurate / not up-to-date ?

What would then be best way to simulate the DC operating point ?

Thanks,

Regards,

0 项奖励
回复