Hello, I want to configure the timestamp function via SJA1105, but if it is used when using filter mode
MAC_FLTRES address of the [0] threshold as the destination address, it seems that it will be discarded, and there is no wait for the META frame, the corresponding setting is as follows, is it necessary to set it elsewhere? Another TCAM setting forwarding rules I also didn't understand, pain, solve! Thank you!