SJA1105 xMII Connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SJA1105 xMII Connection

跳至解决方案
3,469 次查看
harish720
Contributor II

As shown below, in the typical application circuit of SJA1105 ethernet switch IC, I have noticed that a host processor is always connected to one of the xMII ports of the switch and also through an SPI channel. According to the datasheet, the switch IC can be configured through the SPI communication, so why do we need to use up one of the ports to connect to the host processor? Why not use it for another incoming ethernet connection? What advantages do connecting the host processor through xMII interface give us?

harish720_0-1665731623251.png

 

0 项奖励
回复
1 解答
3,445 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

a DS mentions that briefly...

Ethernet connectivity to the host processor is only needed if the system has to support AVB operation or other bridge management protocols such as STP/RSTP. If such operations are not needed, all the
ports can be used for data traffic.

BR, Petr

在原帖中查看解决方案

4 回复数
3,446 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

a DS mentions that briefly...

Ethernet connectivity to the host processor is only needed if the system has to support AVB operation or other bridge management protocols such as STP/RSTP. If such operations are not needed, all the
ports can be used for data traffic.

BR, Petr

3,435 次查看
harish720
Contributor II
Hi,
Thanks for the response.
Just one more doubt, this an automotive grade switch and can be used for GBASE-T1 (single pair ethernet) but if we use an appropriate PHY then we can also use it with full GBASE-T (using all 4 pairs of ethernet) cable for communication right?
0 项奖励
回复
3,427 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I think so

PetrS_0-1666168980234.png

BR, Petr

3,423 次查看
harish720
Contributor II
Thanks for your support Petr.
0 项奖励
回复