SGTL5000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGTL5000

1,280件の閲覧回数
inmaku
Contributor III

To Whom It May Concern:

We use the SGTL5000 in the QFN20 package in our custom iMX6Q design. The data sheet states, that the I2C adderss is fixed at 0x0A - but when we probe the I2C bus, we only see 0x0C !

Even with the 0x0C, we cannot read any matching or reasonable data.

The marking on the chip says:

SG 50

00  X

AADS

My assumption is, that this is an early version of the chip and thus some stuff is different?

Any help and/or clarification appreciated!

Ingo

ラベル(2)
0 件の賞賛
返信
0 返答(返信)