SGMII questions between SJA1110 and PHY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGMII questions between SJA1110 and PHY

591件の閲覧回数
baymax0-0
Contributor I

In the process of using SGMII to establish the communication between NXP SJA1110 and TI's DP83TG720s, we found that the two could not be linked up. I want to know what parameter configuration should be paid attention to in this process. I have paid attention to the rate consistency problem. In addition, will the negotiation time or other parameters affect the establishment of the connection?

Thank you very much!

タグ(3)
0 件の賞賛
返信
1 返信

560件の閲覧回数
kaden
NXP Employee
NXP Employee

Hi baymax0-0,

can you provide further information:

- which hardware are you using? SJA1110EVM or your own design?

- which toolchain do you use to configure the switch? E.g. S32 Design Studio + SDK, NXP Python Tools, EB Tresos.... 

BR

Kevin

0 件の賞賛
返信