SGMII questions between SJA1110 and PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGMII questions between SJA1110 and PHY

468 Views
baymax0-0
Contributor I

In the process of using SGMII to establish the communication between NXP SJA1110 and TI's DP83TG720s, we found that the two could not be linked up. I want to know what parameter configuration should be paid attention to in this process. I have paid attention to the rate consistency problem. In addition, will the negotiation time or other parameters affect the establishment of the connection?

Thank you very much!

0 Kudos
Reply
1 Reply

437 Views
kaden
NXP Employee
NXP Employee

Hi baymax0-0,

can you provide further information:

- which hardware are you using? SJA1110EVM or your own design?

- which toolchain do you use to configure the switch? E.g. S32 Design Studio + SDK, NXP Python Tools, EB Tresos.... 

BR

Kevin

0 Kudos
Reply