SE052 Multiple Session

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE052 Multiple Session

1,634 Views
MohitGediya
Contributor III

Good evening community,
I am creating one zephyr-based project and include Nano-Plug and Trust module.
I use FRDM_KE17z512 board, SE052 IC.

Let me know, can I able to communicate two SE052 ICs(same ICs) at the same time with one Carrier board.
Is this supported with my software and hardware set-up?
Also i want to authenticate crypto object which is non-deletable(remove delete policy at creation time), may i able to read that object again for data encryption.
In that i use AES symmetric key with cbc mode algorithm.

0 Kudos
Reply
6 Replies

1,620 Views
MohitGediya
Contributor III

@Kan_Li , @AnnaKalpa @Twan Please give reply.

0 Kudos
Reply

1,561 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @MohitGediya ,

 

Do you mean you want to communicate with the two SE05xes with the same slave address on the same I2C bus?  Which use case needs two SE ? Please kindly clarify.

 

Best Regards,

Kan

0 Kudos
Reply

1,511 Views
MohitGediya
Contributor III

On same I2C slave address is possible then how to two different operation will perform at same time over 2 different ICs?
Or can I use two different I2C peripherals, What is best option for production?

Can i use one I2C peripheral of physical carrier board?
Can i create two different sessions at same time to communicate with two ICs?

Tags (1)
0 Kudos
Reply

1,505 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @MohitGediya ,

 

I see, but if you want to open two different sessions at same time to communicate with two ICs, please make sure they are on different I2C buses, for example, one SE050 is on "/dev/i2c-1" , and the other is on "/dev/i2c-2".

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,498 Views
MohitGediya
Contributor III

I am use Zephyr rtos based platform, Should i open other session to communicate with ICs?
For each IC communication, should i open dedicated I2C session? How to manage?
@Kan_Li  SE052 Multiple Session 

0 Kudos
Reply

1,458 Views
MohitGediya
Contributor III

If i want to open one AESKey session and one ECKey session in same IC.
Then can i open in two different sessions nano plug and trust module?

@Kan_Li 

0 Kudos
Reply