SE050

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050

1,619件の閲覧回数
tkl_H_890
Contributor I

SE050不焊接有办法写入数据吗? 您好, 我公司想使用SE050保护我们程序,应用场景如下: 我们会将SE050焊接在客户的电路板上,我们的IP也会交给客户的FPGA开发人员让他们一同写入他们的FPGA中。我们的IP中有与SE050的通讯代码,因此我们需要在SE050焊接在客户的PCB之前,就建立与这片SE050的安全通信,并将独特的秘钥/识别代码,写入SE050的存储器,以便客户开机使用的时候,我们IP能够识别到独特的秘钥/识别代码,确保我们的IP仅能在该PCB上使用,不会被无限复制。 我的问题就是:您公司案例里有没有 接触过,在SE050焊接在客户的PCB之前,就能编程并将数据写入SE050的方法,这样客户无法在他们的PCB上对SE050重新编程。

0 件の賞賛
返信
1 返信

1,599件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @tkl_H_890 ,

 

我们有partner提供相关的服务:

Kan_Li_0-1743490086449.png

详见 https://www.nxp.com/products/security-and-authentication/secure-service-2go-platform/edgelock-2go:ED... 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信