SE050 OpenSSL 3 Provider configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SE050 OpenSSL 3 Provider configuration

5,213 次查看
joaoprudencio
Contributor I

Hi,

I'm using OM-SE050ARD with Yocto, OpenSSL 3.0.5, Plug & Trust MW 4.03.01 and have simw-top/sss/plugin/openssl_provider/bin/libsssProvider.so file and now I would like to know what changes I need to do in openssl.cnf file to use OpenSSL lib as SE050 Provider and after that what is the easy way to check the solution ?

Thank you in advance,

Joao

 

0 项奖励
回复
6 回复数

5,173 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @joaoprudencio ,

 

There is no need to edit openssl.cnf, OpenSSL 3 Provider can be used directly out of box. Please kindly refer to SE05x-MW-v04.03.01/simw-top/doc/sss/plugin/openssl_provider/scripts/readme.html for details. We also provide some scripts for test purpose. You may refer to "simw-top/sss/plugin/openssl_provider/scripts" for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,005 次查看
mgrand
Contributor II

Dear Kan_Li,

I still have the exact same question, how is it possible to configure the se050 provider from openssl config file ? I'm using a third party software (which cannot be modified) which is based on openssl to handle a TLS network connection. 

At the moment, I have a semi working setup where the se050 provider seems to completely "hide" the default openssl provider therefore I'm not able to setup a working connection as the se050 provider does not implements all the algorithms needed to setup a TLS connection.

Can you provide me a working configuration file which handles the fallback to the built-in openssl algorithms when an algorithm is not implemented by your provider?

Best regards

0 项奖励
回复

4,969 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @mgrand ,

 

As far as I know, such config file is just used for TLS use case in openssl 1.1 / 1.0, while TLS use case is not yet supported for openssl 3.0. So no such config files are present.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,732 次查看
rhuber
Contributor II
What is the recommended way to communicate with Azure using the TPM?

I summarized my findings in this question of the azure c sdk: https://github.com/Azure/azure-iot-sdk-c/issues/2657
0 项奖励
回复

5,139 次查看
joaoprudencio
Contributor I

Thank you for your quick answer and I have a one more question.

When I run the script "python3 openssl_rnd.py" everything ends correct, but when I run " python3 openssl_provisionEC.py --key_type prime256v1" at the end I get the following errors:

###############################################################
#
# SUBSYSTEM : se05x
# CONNECTION_TYPE : t1oi2c
# CONNECTION_PARAMETER : none
#
###############################################################
smCom :ERROR:Failed writing data (nrWritten=-1).

smCom :ERROR: - Error in I2C Write.....
smCom :ERROR:phNxpEseProto7816_SendRawFrame Error phNxpEse_WriteFrame
smCom :ERROR:TransceiveProcess Transceive send failed, going to recovery!
smCom :ERROR:phNxpEseProto7816_Open failed
smCom :ERROR: Failed to Open session
sss :ERROR:SM_I2CConnect Failed. Status 7012
# Connection parameters:
# subsystem : se05x
# connection_type : t1oi2c
# connection_data : none

 

My question it's what could be the reason for these errors ?

 

Thank you in advance

Joao

 

0 项奖励
回复

5,097 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @joaoprudencio ,

 

Actually I haven't met such kind of issue before, and I am not sure if there is enough space left in your OM-SE050ARD, but maybe you can try to run se05x_Delete_and_test_provision at first. Please kindly let me know if the problem is still there.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复