Hello,
We are facing SC18IS602B I2C to SPI bridge Latch-Up issue after power down system (from S0-S5-G3).
The failure rate is around 0.26% (4pcs out of 1500pcs)
We take this part in Intel x86 platform to convert data from embedded controller IT5121VG to battery charger LTC1960CG#TRPBF (SS0#).
It was found the VDD(3.3V) has voltage remained (0.3V) during power off. It needs to take a time for fully discharging remained power.
The latch-up occurred after next power up with VDD remaining power 0.3V. The failure rate is not 100% but close to 10%.
Pulling RESET# signal to low cannot fix latch-up issue when problem occurred.
We would like to clarify some items:
1) What's the latch-up condition of this part ?
2) What's the voltage threshold of power on reset(POR) for this part ?