SC18IS602 - SPI Timing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SC18IS602 - SPI Timing

2,587 次查看
JoergS
Contributor I

Hello,

I use a SC18IS602 in my application.

I have analyzed I2C and SPI communication with a logic analyzer. After a I2C command to transmit some bytes on the SPI bus is received, the device starts transmitting the bytes on the SPI bus.

I am wondering why there is a delay of 8.8µs between the sent bytes on the SPI bus? The SPI clock is 1843 kHz. I have attached a screenshot

Greetings

Joerg

0 项奖励
回复
3 回复数

2,581 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jörg,

 

I do not have the design specifications and cannot explain that since this device is pretty old (2006). However, based on our measurements, the idle time between the sent bytes is indeed around 9us when the SPI clock is at 1.8MHz. 

 

Best regards,

Tomas

0 项奖励
回复

2,577 次查看
JoergS
Contributor I

Thank you for your reply

The effective transfer rate is just approximately one-third. This is too slow in my application. I knew that I2C is much slower but I have to read out the data of a SPI slave with more than 1MHz because otherwise the data would be corrupted.

Is there a newer I2C to SPI bridge in your portfolio?

 

0 项奖励
回复

2,570 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jörg,

 

Unfortunately there are not any newer I2C to SPI bridges in our portfolio.

 

Best regards.

Tomas

0 项奖励
回复