SC18IM704 UART message rate

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SC18IM704 UART message rate

1,419 次查看
Tix00
Contributor II

Hi to everyone! wich is the maximum message rate (I2C transactions) for this IC?

标记 (2)
0 项奖励
回复
2 回复数

1,394 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Vicent,

The I2C clock rate is configurable via I2CClkL and I2CClkH registers and can be set up to 375 kHz.

Capture.JPG

BR, Tomas

0 项奖励
回复

1,391 次查看
Tix00
Contributor II

Hi Tomas, thanks for your fast reply.

Your table referes to I2C bus clock frequency, but my question is about the overall IC capacity for processing UART messages to the I2C machine. I mean to send a simple (two bytes) SxxxxxxP I2C write [not waiting for an answer] command message to the UART interface and dump it to the I2C bus.

Thank you in advance!

0 项奖励
回复