SC18IM700 TX-Line Driving Issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC18IM700 TX-Line Driving Issues

1,138 Views
benjaminwyrsch
Contributor I

We are using the SC18IM700 in our design.

We have detected that the TX-line shows some artifacts during the rising and the falling slope.

What is the reason for these artifacts?

Is the output driver that weak?

There is an external 10kOhm pull-up resistor in the TX-line.

I don't think that this resistor causes the artifacts.

I also couldn't find any electrical specification of the TX-line output in the datasheet.

Can anybody provide the electrical specification and detailed information about the electrical output circuit (open-drain, push-pull, etc)?

Thanks

Benjamin

Tags (2)
0 Kudos
Reply
2 Replies

925 Views
david_diaz
NXP Employee
NXP Employee

Hello Benjamin,

The pull-up at the TX line could slightly prolong the signal’s fall time. Have you considered to remove or decrease the pull-up resistor?

If you remove the resistor, does the signal behave correctly? Could you please share your results?

Regards,

David

0 Kudos
Reply

925 Views
benjaminwyrsch
Contributor I

We have found the reason for the artifacts: We were using a bidirectional level-shifter IC for the TX and RX lines. This level shifter doesn't work properly with slow slopes resp. open-drain circuits. We have replaced this IC with direction controlled buffers. All is good now.

0 Kudos
Reply