SC18IM700 Input Supply Maximum

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SC18IM700 Input Supply Maximum

1,348 次查看
graeme_anderson
Fresh Out Contributor

I have to interface with an I2C device that uses 5V levels.

The SC18IM700 is not interpretting the acknolegment as its Vil = 0.3 * Vdd. Can i operate the SC18IM700 from 5V?

Cheers

G

标记 (3)
0 项奖励
回复
1 回复

1,310 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Graeme,

The operating VDD is 2.4V to 3.6V. You would need a level shifter to interface the device to a 5V I2C master. Or, the pull up the I2C bus to 3.3V instead of 5V.

Best regards,

Tomas

0 项奖励
回复