SC16IS762

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC16IS762

1,386 Views
qdinh
Contributor I

What is the max frequency for the XTAL input of SC16IS762?  The datasheet only shows the max baud rate for the serial interface up to 5Mbps.  Per the formula for the baud rate, can I assume the max freq for the XTAL input is 60MHz?

Tags (2)
0 Kudos
Reply
1 Reply

1,374 Views
guoweisun
NXP TechSupport
NXP TechSupport

VDD=2.5V support to Max 48MHz.

VDD=3.3V support to Max 80MHz

0 Kudos
Reply