SC16IS760 LSR: 0x08 error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC16IS760 LSR: 0x08 error

1,206件の閲覧回数
Martin10
Contributor I

Dear Sir/Madam,

We are using SC16IS760 to convert UART signals to SPI signals which are routed to a MCU.

We noticed that occasionally (< 1% of the time), we will see 0x08 error during data streaming.

The datasheet mentioned this is "framing error".

Based on your experience, would this be likely caused by clock mismatch between RX and TX of the UART interface? As this happens not very frequently, any suggestion on how to narrow down the root cause? Appreciate your insight!

Best regards,

Martin

@guoweisun 

0 件の賞賛
返信
1 返信

1,190件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

1: can you share with the schematic?

2: Is possible to catch the waveform when error happened?

 

0 件の賞賛
返信