SC16IS752IPW

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SC16IS752IPW

1,674 次查看
kame
Contributor I

I use SC 16 IS 752 IPW, but if I communicate with 2 channels simultaneously, I lose data.
Also, an overrun error has occurred.
What could be the cause?

0 项奖励
回复
1 回复

1,576 次查看
darioarias
NXP Employee
NXP Employee

Hello,

The two channels share the same FIFO inside the bridge, therefore if you are using both simultaneously it can cause overwrite of the data. Also overrun errors occur if the transmit data rate exceeds the receive FIFO servicing latency that will occur if you are accessing the FIFO with the 2 channels at the same time, but it's hard to tell if that is the reason of your issue. Could you share the configuration you used?

Regards,

Darío

0 项奖励
回复