SC16IS750 under 4.4.120 kernel CANNOT transmit file to the other pear

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC16IS750 under 4.4.120 kernel CANNOT transmit file to the other pear

1,610 Views
JarvisC
Contributor II

Hi NXP sir,

We develop SC16IS750 as we RS485 UART data source from our SoC.

We met problem that we can receive the file from other pear

But we cannot transfer the file and get similar time out message on tool

Could you share some suggestion for this problem?

Thanks all

Case

BPS

Direction

Size

Flow control

Result

Message from Tool

1

9600

RX

10K

SW

Pass

EFR=0x0A

2

9600

RX

64B

SW

Pass

EFR=0x0A

3

9600

RX

63B

SW

Pass

EFR=0x0A

4

9600

TX

63B

SW

Fail

 

5

115200

RX

63B

SW

Pass

EFR=0x0A

6

115200

RX

64B

SW

Pass

 

7

115200

RX

65B

SW

Pass

 

8

115200

RX

10K

SW

Fail

Timeout

9

115200

RX

128B

SW

Pass

 

10

115200

RX

129B

SW

Fail

Timeout

11

115200

RX

192B

SW

Fail

RX FIFO overrun/timeout

 

JarvisC_1-1649729129258.jpeg

 

 

 

0 Kudos
Reply
8 Replies

1,589 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jarvis,

please state your Annual Volume for this project. Please see below an answer from an application engineer I have contacted.

DESCRIPTION

For such as low volume I don’t think we can provide much support. The customer need to debug issue on its own.

 

  1. Hook up a logic analyzer to the I2C or SPI bus and the device TX/RX pins. Watch for the code to send data to the SC16IS750.
  2. Does the code that attempt to send the data is correct? Send something sensible like 0, 1, 2, 3, 4, 5
  3. Does to code send these data to the transmit FIFO?
  4. Does anything come out of the TX pin?
  5. Does the TX signal come all the way out to the RS232/485 cable?

 

Any data the come into the TXFIFO will be automatically send out on the TX pin.’

With Best Regards,

Jozef

0 Kudos
Reply

1,583 Views
JarvisC
Contributor II

Hi Jozef,

Please kindly review below information, and share your suggestion.

  1. Hook up a logic analyzer to the I2C or SPI bus and the device TX/RX pins. Watch for the code to send data to the SC16IS750.

[4/13,Ans:]We had setting I2C LA for SCL/SDA

  1. Does the code that attempt to send the data is correct? Send something sensible like 0, 1, 2, 3, 4, 5

[4/13,Ans:]We had used to type character from keyboard success but cannot transfer file

  1. Does to code send these data to the transmit FIFO?

[4/13,Ans:]Should be YES base of above answer we type character is success

  1. Does anything come out of the TX pin?

[4/13,Ans:] TX waveform is available on scope, but cannot make sure data incorrect

  1. Does the TX signal come all the way out to the RS232/485 cable?

[4/13,Ans:] The TX /RX will connect to level shift and RS485 transceiver

 

Thanks.

0 Kudos
Reply

1,576 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jarvis,

could you please provide the Annual Volume for your project? Or is the project (and the Annual Volume) not defined yet? 

With Best Regards,

Jozef

0 Kudos
Reply

1,566 Views
JarvisC
Contributor II

Hi Jozef,

After checked the Annual Volume for the project, it's about 10k/yr for 5 years.

Thanks.

0 Kudos
Reply

1,515 Views
JarvisC
Contributor II

Hi Jozef,

Could you share some suggestion that could help us to fix the problem?

Thanks.

0 Kudos
Reply

1,486 Views
JarvisC
Contributor II

Hi Jozef,

Is there any updated information about our questions?

Please help to share your suggestion.

Thanks.

0 Kudos
Reply

1,483 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jarvis,

I apologize for a late reply. We had two days off due to Easter holiday. This morning I have sent your answers to the application engineer. As soon as I will receive an answer from him, I will definitely reply to you.

Thank you for your patience.

With Best Regards,

Jozef

0 Kudos
Reply

1,468 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jarvis,

I have bad news. The application engineer has sent me an answer. Please see below. I apologize for inconvenience.

DESCRIPTION

I can not offer any help without looking at the actual scope shot to show exactly what is happening. As I said before, for such a low volume the customer need to debug his own issue.

With Best Regards,

Jozef

0 Kudos
Reply