SC16IS750 problem to verify TX/RX functionality

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SC16IS750 problem to verify TX/RX functionality

1,354 次查看
jedward1977
Contributor I

Hi

I have a simple project with this IC.

I just configured the product to work as I2C - UART.

But when I write in the THR register, I expect the TXLVL register needs to show some number related to number of spaces available. But this register is always with the same number.

I am using a Raspberry to send the I2C commands, and I read all related documentation and follow the order of the commands this forum suggests but I am not having success.

"""
self.bus.write_byte_data(self.DEVICE_ADDRESS, LCR, 0x80)
 
# Set DLL
self.bus.write_byte_data(self.DEVICE_ADDRESS, DLL, 0x78)

# Set DLH
self.bus.write_byte_data(self.DEVICE_ADDRESS, DLM, 0x00)

print("Set 0xBF")
self.bus.write_byte_data(self.DEVICE_ADDRESS, LCR, 0xBF)

# EFR only can be accessed with LCR = 0xBF
# EFR[4] --> enable enhanced functions
self.bus.write_byte_data(self.DEVICE_ADDRESS, EFR, 0x10)
 
# 8 data bit, 1 stop bit, no parity
self.bus.write_byte_data(self.DEVICE_ADDRESS, LCR, 0x03)

# FCR: 0 0 1 0 0 1 1 1
self.bus.write_byte_data(self.DEVICE_ADDRESS, FCR, 0x27)

"""

Log of execution:

Line Status LSR (hex): 0x60
Modem status MSR (hex): 0x0
TXLVL (hex): 0x40
RXLVL (hex): 0x0

Writing DATA to THR: 0xfa
Reading DATA (hex) from RHR:  0x19
Line Status LSR (hex): 0x60
Modem status MSR (hex): 0x0
TXLVL (hex): 0x40
RXLVL (hex): 0x0

Writing DATA to THR: 0xfb
Reading DATA (hex) from RHR:  0x19
Line Status LSR (hex): 0x60
Modem status MSR (hex): 0x0
TXLVL (hex): 0x40
RXLVL (hex): 0x0

 

As you see, there is no changes in the Status or Tx/Rrx registers.

Do you have some idea of how to debug this?

I saw TX pin is always high. But the configuration is OK.

Regards

 

0 项奖励
回复
1 回复

1,332 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Here I attached the SPI reference code,hope this could help you!

 

0 项奖励
回复