SC16IS741A with a different crystal from example.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC16IS741A with a different crystal from example.

2,145件の閲覧回数
guillep2k
Contributor I

I'd like to use SC16IS741A with an SMD crystal (i.e., not 1.8432 MHz); something like ABLS-LR-3.072MHZ-T (18pF load capacitance) or smaller.

If possible, what values should I use for C1/C2 which should be 0805 on a 2-layer PCB?

0 件の賞賛
返信
3 返答(返信)

2,015件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Guillermo,

Yes, you can use the the 3.072 MHz or smaller crystal and the C1/C2 value are 22/33 pF.

picture_5.png

Best regards,

Tomas

2,015件の閲覧回数
guillep2k
Contributor I

Thank you, Tomas; I see I can still use the capacitor values given for the 1.8432 MHZ crystal. Is there a range of crystal frequencies I could use? Like 11.0592 MHz or others, in case I need further miniaturization of my design? How can I calculate the right capacitors in those cases?

Kind regards,

Guillermo

0 件の賞賛
返信

2,015件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Guillermo,

The datasheet specifies the crystal oscillator max. 24 MHz and it is okay to use both C1/C2 as 22/33 pF.

Best regards,

Tomas

0 件の賞賛
返信