SBC:F6500

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SBC:F6500

1,186 次查看
Wen666
Contributor II

Currently, I am encountering a problem related to the DIAG_SF_ERR_ADR register during the initialization of the FS6522 chip. The specific situation is as follows: after completing LBIST and ABIST1, the self-check shows "OK" and the fault count of the DIAG_SF_ERR_ADR register is 0. However, after reading the next register (regardless of which one is read), the fault count of the DIAG_SF_ERR_ADR register becomes 5. Have any of you encountered the same problem? I'm seeking an answer and haven't been able to identify the cause yet.

Wen666_1-1751267598565.pngWen666_2-1751267751893.png

 

 

标记 (2)
0 项奖励
回复
4 回复数

1,173 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Does this problem happen also in Debug mode? If not, my assumption is that there is WD refresh error that increases the fault error counter in such a short time. Please try to use the initialization sequence shown in our AN5238, chapter 14.2.

BRs, Tomas

0 项奖励
回复

1,161 次查看
Wen666
Contributor II

Thanks.
It will also occur in the debugging mode. Further investigation revealed that this situation only occurs during the first run after the program is burned. After a restart, the error fault count returns to normal. The initialization process follows the manual and involves reading and writing to the registers.

0 项奖励
回复

1,154 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Is there watchdog refresh before fault error counter readout 0? How many times ? There will be several external RSTB during MCU program that leading to fault error counter increase. So I wonder fault error counter 5 is right and 0 is not right?

To see details, please share SBC SPI commands for analysis.

BRs, Tomas

0 项奖励
回复

1,149 次查看
Wen666
Contributor II

Here is my initialization process code. During the initialization process, no reset occurred. According to the data manual, the error fault counter should be 1 in the initialization stage if no fault occurred. It should be reduced to 0 after seven correct dog-feeding operations. The dog-feeding process was normal, but the value read from the fault error counter was 5 instead of 1.

void FS65_Init(void)
{
uint8_t WDRefresh = 0;
uint32_t fs65_error_code = 0;

// 0- Get silicon version
/*fs65_error_code = FS65_UpdateRegisterContent(DEVICE_ID_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_DEVICE_ID);*/

// 1- Verify
// Built-in self-test
fs65_error_code += FS65_UpdateRegisterContent(BIST_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_BIST);
if(0 == INTstruct.BIST.B.LBIST_OK)
{
FS65_ErrorCallback(); // Logic built-in self-test
}

if(0 == INTstruct.BIST.B.ABIST1_OK)
{
FS65_ErrorCallback(); // Analog built-in self-test
}

// Verify VPRE buck or buck boost configuration
// Verify VCCA and VAUX voltage configuration (3.3 V or 5.0 V)
// Verify debug mode is not activated
// Verify deep Fail-safe configuration
fs65_error_code = FS65_UpdateRegisterContent(HW_CONFIG_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_HW_CONFIG);

// 2- Configure
// Configure VCORE, VCCA, and VAUX overvoltage and undervoltage impact on RSTB and FS0B
fs65_error_code = FS65_Set_INIT_VCCA_OVUV_IMPACT(FS65_Registers_InitValues.INIT_VCCA_OVUV_IMPACT);

fs65_error_code = FS65_Set_INIT_VCORE_OVUV_IMPACT(FS65_Registers_InitValues.INIT_VCORE_OVUV_IMPACT);

fs65_error_code = FS65_Set_INIT_VAUX_OVUV_IMPACT(FS65_Registers_InitValues.INIT_VAUX_OVUV_IMPACT);

// Configure VAUX as tracker of VCCA if using VAUX to supply sensors and VCCA as an
// MCU ADC reference voltage
fs65_error_code = FS65_Set_INIT_VREG(FS65_Registers_InitValues.INIT_VREG);
FS65_Check_Error(fs65_error_code, FS65_errorcode_INIT_VREG);

// Configure the WD window period and the WD counters
fs65_error_code = FS65_ChangeWDwindow(FS65_Registers_InitValues.WD_WINDOW);
FS65_Check_Error(fs65_error_code, FS65_errorcode_WD_WINDOW);

// Configure the final and indirectly intermediate value of the fault error counter
fs65_error_code = FS65_Set_INIT_WD_CNT(FS65_Registers_InitValues.INIT_WD_CNT);
FS65_Check_Error(fs65_error_code, FS65_errorcode_INIT_WD_CNT);

// Configure the WD impact on RSTB and FS0B
fs65_error_code = FS65_Set_INIT_SF_IMPACT(FS65_Registers_InitValues.INIT_SF_IMPACT);
FS65_Check_Error(fs65_error_code, FS65_errorcode_INIT_SF_IMPACT);

// Configure RSTB and FS0B behavior when fault error counter intermediate value
fs65_error_code = FS65_Set_INIT_FAULT(FS65_Registers_InitValues.INIT_FAULT);
FS65_Check_Error(fs65_error_code, FS65_errorcode_INIT_FAULT);

// Configure the RSTB pulse duration
// Configure MCU FCCU error monitoring in regards to IO[2] and IO[3] connections
// Configure Ext. IC error monitoring in regards to IO[4] and IO[5] connections
fs65_error_code = FS65_Set_INIT_FSSM(FS65_Registers_InitValues.INIT_FSSM);
FS65_Check_Error(fs65_error_code, FS65_errorcode_INIT_FSSM);

fs65_error_code = FS65_Set_INIT_WU1(FS65_Registers_InitValues.INIT_WU1);
FS65_Check_Error(fs65_error_code, FS65_errorcode_INIT_WU1);

fs65_error_code = FS65_Set_INIT_WU2(FS65_Registers_InitValues.INIT_WU2);
FS65_Check_Error(fs65_error_code, FS65_errorcode_INIT_WU2);

// 3- Execute
// Execute ABIST2 on VAUX by the SPI request from the MCU
fs65_error_code = FS65_UpdateRegisterContent(INIT_VAUX_OVUV_IMPACT_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_INIT_VAUX_OVUV_IMPACT);
if((INTstruct.INIT_VAUX_OVUV_IMPACT.B.VAUX_FS_OV) || (INTstruct.INIT_VAUX_OVUV_IMPACT.B.VAUX_FS_UV))
{
fs65_error_code = FS65_RunABIST2_VAUX();
FS65_Check_Error(fs65_error_code, FS65_errorcode_ABIST2_VAUX);
}

fs65_error_code = FS65_UpdateRegisterContent(BIST_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_BIST);
if(0 == INTstruct.BIST.B.ABIST2_VAUX_OK)
{
FS65_SetLPOFFmode_autoWU();
FS65_ErrorCallback();
}

// Close the Fail-safe INIT phase
FS65_WD_Refresh();

// Close the Main INIT phase
fs65_error_code = FS65_Set_INIT_INT(FS65_Registers_InitValues.INIT_INT);
FS65_Check_Error(fs65_error_code, FS65_errorcode_INIT_INT);

// Clear all the flags by reading all DIAG registers of both Main and Fail-safe registers
// Main registers
fs65_error_code = FS65_UpdateRegisterContent(DIAG_VPRE_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_DIAG_VPRE);

fs65_error_code = FS65_UpdateRegisterContent(DIAG_VCORE_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_DIAG_VCORE);

fs65_error_code = FS65_UpdateRegisterContent(DIAG_VCCA_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_DIAG_VCCA);

fs65_error_code = FS65_UpdateRegisterContent(DIAG_VAUX_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_DIAG_VAUX);

fs65_error_code = FS65_UpdateRegisterContent(DIAG_VSUP_VCAN_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_DIAG_VSUP_VCAN);

fs65_error_code = FS65_UpdateRegisterContent(DIAG_SPI_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_DIAG_SPI);

// Clear the fault error counter to "0" by seven consecutive good WD refresh
for(WDRefresh = 0; WDRefresh < 7; WDRefresh ++)
{
Loncin_Dealy_ms(1);
FS65_WD_Refresh();

// Refresh the failure error counter
fs65_error_code = FS65_UpdateRegisterContent(DIAG_SF_ERR_ADR);
}

// 6. Configure parameters for the non-init_in phase
fs65_error_code = FS65_Config_NonInit();
FS65_Check_Error(fs65_error_code, FS65_errorcode_NonInit);

// 7. Release FS0B (active high)
fs65_error_code = FS65_UpdateRegisterContent(RELEASE_FSxB_ADR);
FS65_Check_Error(fs65_error_code, FS65_errorcode_RELEASE_FSxB);

FS0B = INTstruct.RELEASE_FSxB.B.FS0B_SNS;
fs65_error_code = FS65_ReleaseFS0B();
FS65_Check_Error(fs65_error_code, FS65_errorcode_ReleaseFS0B);

// Configure the WD window period to 1024ms
fs65_error_code = FS65_ChangeWDwindow(WD_WIN_1024);
FS65_Check_Error(fs65_error_code, FS65_errorcode_WD_WINDOW);
}

0 项奖励
回复