SAC57D54HCVLTR cannot be flashed on the first time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SAC57D54HCVLTR cannot be flashed on the first time

2,661件の閲覧回数
johnkevintoral
Contributor II

Hello, 

I have made a custom board with SAC57D54HCVLTR 208-pin MCU; however, the first time it is powered, it is in the reset state, is this normal?

And I have tried to flash it using S32DS for Arm, but it is not working. The IDE says 'cannot communicate with the board'. I have been using its eval board for the past 2 years, the MAC57D54MB but with the BGA version of the said MCU, and I assure all settings in the IDE are correct. 

I have checked the schematics and PCB, and it is all well. I use JTAG, btw.

Any ideas on how to load the MCU for the first time would greatly help. 

Thank you.

0 件の賞賛
返信
5 返答(返信)

2,524件の閲覧回数
johnkevintoral
Contributor II

Hi 

I found a mistake in my custom board where the 2 external clocks are far enough from the MCU. Will definitely fix this. Will update soon. 

Thanks. 

0 件の賞賛
返信

2,572件の閲覧回数
johnkevintoral
Contributor II

Hi,

It seems to me that the current state is the Powerup phase where the MCU is stuck. I have checked all power supplies with 1.2V and 3.3V which are all okay. Anyone with same experience?? what could possibly be the reason for this? thanks

0 件の賞賛
返信

2,641件の閲覧回数
johnkevintoral
Contributor II

Hi Bio_TICFSL,

I have checked all switches and power supply, and they are fine. My first question was the MCU supposed to be in a reset state upon first powering up? thanks

0 件の賞賛
返信

2,619件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

yes

0 件の賞賛
返信

2,649件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

You must check the fuses or the Switches to stay in flash to program then to run, you can program this with JTAG as well.

This product is out of support please check it replacement:

https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-rt595-eval...

 

Regards

 

 

 

0 件の賞賛
返信