S32Z/E

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32Z/E

345件の閲覧回数
TXJ
NXP Employee
NXP Employee

Hi,

I am using a Greenbox daugtherboard(DC4) with a S32E278 chip and I want to use the R52 core. I am trying to run simple drivers within Design Studio 3.5 in the peripheral tool. I am using the CodeWarrior TAP debugger to flash my code. Nevertheless in the  "SW32ZE_RTD_R21-11_0.9.0_Po1_D2211_DS_updatesite" SDK there are limited examples for the S32E278 chip. 

Do you have some documentation about how to use the RTD together with the S32E278 chip in the peripheral tool in Design Studio 3.5?

0 件の賞賛
返信
0 返答(返信)