S32 Debug Probe Run/Pause LED is red

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Debug Probe Run/Pause LED is red

2,140件の閲覧回数
ahmedgheith
Contributor III

I have the S32 Debug Probe connected to the S32V234 SBC evaluation board. Sometimes when I restart the board, the Run/Pause LED on the Debuge Probe becomes red.

In this case I can still run codes on the board through S32DS. But should I be concerned? What should I do in this case?

Thank you.

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,115件の閲覧回数
bpe
NXP Employee
NXP Employee

The status indicated by S32 Debug Probe LEDs is explained on page 17 of
S32 Debug Probe User Guide. You can find this document under
S32DS\tools\S32Debugger\Debugger\Docs\ . The path is from your S32DS
installation directory.

Best Regards,
Platon

 

0 件の賞賛
返信

2,089件の閲覧回数
ahmedgheith
Contributor III

Hi @bpe ,

 

Thank you for your reply.

I saw this page before posting my question. To my understanding, these modes should only change if some change is applied to the target board (for example: running a program on one of the cores of the board), right?

But I noticed that if the debug probe is restarted (turned off then turned on again) while keeping the target board as it is, this can change the mode from Run to Pause. Is this normal? And does this mean I can't run a debug session then?

 

Also how can I change the mode of the target board from Pause/Mix to Run?

 

Best regards,

Ahmed Gheith

0 件の賞賛
返信