Rotary Encoder Interfacing with PCAL9722

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rotary Encoder Interfacing with PCAL9722

650 Views
mk031
Contributor I

We are going to use Rotary incremental Encoder (Quadrature output) via SPI to IO Expander.

As Rotary Encoder requires Interrupt pin to interface, can you please Confirm whether it is possible to interface Rotary Encoder with PCAL9722 I/O Expander?

Does PCAL9722 supports interrupt on Rising as well as falling edge?

Thanks in advance!

0 Kudos
Reply
1 Reply

625 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Yes, the PCAL9722 supports interrupt functionality that can be configured by level or edge, and each interrupt can be cleared individually without affecting other interrupt events.

For more details, please refer to Section 6.4.12 – Interrupt Edge Registers (60h to 65h) in the datasheet.

Hope this helps!

 

 

0 Kudos
Reply