Requesting MMPF0100F2AEP pin library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Requesting MMPF0100F2AEP pin library

2,643件の閲覧回数
Amiraroslan
Contributor I

Hi, 

May need help to provide the pin library of MMPF0100F2AEP for boundary scan test purposes. 

0 件の賞賛
返信
3 返答(返信)

2,621件の閲覧回数
Amiraroslan
Contributor I

Hi Tomas,

It is a file that contains information about the pins of a device, such as the pin name, location, function, and connectivity. We need it to be used in boundary scan testing to configure and use the boundary scan test features. It may be in the XML or Txt format.

I attached the example. 

0 件の賞賛
返信

2,600件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Amira,

Thanks for the additional information and example. I have forwarded them to our product group and they confirmed that there is not such a file/library available.

BR, Tomas

0 件の賞賛
返信

2,625件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Amira,

I am not sure what exactly you are looking for, can you please share more details about your requirement or an example? Is not the pin map and pins description in datasheet sufficient?

BR, Tomas

0 件の賞賛
返信