Request for FFF Replacement for RF Amplifier Gain Block Part Number SBB1089Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for FFF Replacement for RF Amplifier Gain Block Part Number SBB1089Z

1,282 Views
jleu64
Contributor I

Hey NXP community, I am trying to look for a FFF replacement for a gain block amplifier. The part we are currently using is part number SBB1089Z that is currently obsolete. Does NXP offer a FFF alternative?

See datasheet in the mouser link below as well as the attachment:

https://www.mouser.com/ProductDetail/Qorvo/SBB1089Z?qs=p6lVfQR1GSqn6Xv87QE3bg%3D%3D&srsltid=AfmBOorM...

 

1 Reply

1,271 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Please check our General Purpose Amplifier MMG3014NT1 that It is suitable for applications with frequencies from 40 to 4000 MHz.

  • Single 5 Volt Supply
  • P1dB: 25 dBm @ 900 MHz
  • Small-Signal Gain: 19.5 dB @ 900 MHz
  • Third Order Output Intercept Point: 40.5 dBm @ 900 MHz
  • SOT-89 Surface Mount Package
  • RoHS Compliant

Hope this helps.

0 Kudos
Reply