https://www.ebay.com/itm/135621943756?mkevt=1&mkpid=2&emsid=e90001.m161799.l174484&plmtId=700008&mes... Hi,
I have 2K watt FM broadcast transmitter with (2) 1K Pallets with BLF188XR. One is defective and I need to change it out. I found this one in the link, but have no information on it. I'm wondering if I can use the one pictured in place of it to replace the defective one. I don't know if anyone can recognize it or not, but any help would be greatly appreciated.