Replacement AM receiver IC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Replacement AM receiver IC

3,005 Views
grant_taylor
Contributor I

Hi,

I am looking for replacement device for A244D, TCA440 or the MC13030, these all contains controlled RF stage, mixer, separated oscillator and IF amplifier, where the MC13030 is a dual conversion AM receiver.

Thanks

Grant

Labels (1)
  • RF

0 Kudos
Reply
1 Reply

2,816 Views
LPP
NXP Employee
NXP Employee

NXP no longer offers analog AM receivers similar to A244D, TCA440 or the MC13030.

We have software-defined radio devices like TEF668X, TEF665X. They support AM receiver covering LW, MW and full SW bands.

AM/FM Radio and Audio | NXP 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later

point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply