Regarding the issue of S32R series radar processing chips

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding the issue of S32R series radar processing chips

ソリューションへジャンプ
292件の閲覧回数
Esther
Contributor I

May I ask if the S32R294 or S32R41 chips can be used for linear frequency modulation continuous wave radar applications in other bands besides millimeter wave radar?

0 件の賞賛
返信
1 解決策
271件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

 

The processors are not constrained like this

As long as the radar front-end device has compatible MIPI-CSI2/DPHY interface then it can be connected to S32R

Best regards,

Peter

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
272件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

 

The processors are not constrained like this

As long as the radar front-end device has compatible MIPI-CSI2/DPHY interface then it can be connected to S32R

Best regards,

Peter

0 件の賞賛
返信