Regarding the issue of S32R series radar processing chips

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding the issue of S32R series radar processing chips

Jump to solution
255 Views
Esther
Contributor I

May I ask if the S32R294 or S32R41 chips can be used for linear frequency modulation continuous wave radar applications in other bands besides millimeter wave radar?

0 Kudos
Reply
1 Solution
234 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

 

The processors are not constrained like this

As long as the radar front-end device has compatible MIPI-CSI2/DPHY interface then it can be connected to S32R

Best regards,

Peter

View solution in original post

0 Kudos
Reply
1 Reply
235 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

 

The processors are not constrained like this

As long as the radar front-end device has compatible MIPI-CSI2/DPHY interface then it can be connected to S32R

Best regards,

Peter

0 Kudos
Reply