Regarding PF3000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding PF3000

1,727 Views
niteshsahay
Contributor III

Hi

In PMIC PF3000 one pin VDDIO is an Input pin or an output pin.

Regards

Nitesh

0 Kudos
Reply
1 Reply

1,611 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Nitesh,

 

VDDIO is an input pin as can be seen in Table 2 on page 9 of the datasheet.

 

VDDIO is the supply for the digital communication of the device (I2C interface voltage).

You should bypass it with 0.1 µF ceramic capacitor.

Connect to 1.7 to 3.6 V supply and ensure that VDDIO is always lesser than or equal to VIN.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------