RW612-GPIO Pin Conflicts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RW612-GPIO Pin Conflicts

2,056 Views
wima88
Contributor III
Hello,

While running the SCTimer example, I noticed some duplicated GPIOs in the quick start guide:

Connector Pin # GPIO #
J2452
J4552
J543
J133

It appears that for the example, J5 pin 4 should correctly correspond to GPIO 3. Is there a resource where I can find the accurate pinout information?

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,275 Views
AndrewChuang
Contributor I

They are not conflicted -- one is for GPIO_2_FC0_I2S_DATA and the other is for GPIO_2_FC0_UART_RXD_ME, as shown in the FRDM-RW612-SCH.pdf. Thanks to your post, I spotted the difference. I've spent almost a week trying to figure out why my usart had no output... 

0 Kudos
Reply

1,972 Views
wima88
Contributor III

Yes

0 Kudos
Reply

2,031 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Are you using the FRDM-RW612?

Regards,

Daniel.

0 Kudos
Reply